How to ConfigurationPE micro JTAG?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to ConfigurationPE micro JTAG?

7,007 Views
kbj8941
Contributor I

Hi Reader,

I have a S21K144EVB and a PE micro Multilink universal. 

I just want set up JTAG Debug without openSDA. 

I want to know configuration at S32 Design Studio for ARM Version 2018.R1.

I attach the setting image.  

0 Kudos
Reply
5 Replies

6,876 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

it looks that you have swapped out JTAG cable. PIN #1 is on the Right side, not on the left as your image shows. 

Jiri 

0 Kudos
Reply

6,877 Views
kbj8941
Contributor I

Hi, Jiri

Thanks for reply.

I have some question,

 when don't it have openSDA schematic, how can i debbuger configuration using the multilink unviersal Fx with S32 studio?

0 Kudos
Reply

6,877 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

Just choose Multilink FX probe in Debug configurations and connect JTAG cable. Make sure, that you have power for MCU (external 12V power supply or USB) - for USB J107 - shorted 2-3, for external power supply J107 - shorted 1-2 .

Jiri

0 Kudos
Reply

6,877 Views
kbj8941
Contributor I

i missed attach the image.

untitled.png

0 Kudos
Reply

6,877 Views
kbj8941
Contributor I

Hi,  Jiri

Thanks for reply.

i did it this problem!

but i have another prlblem. i need a your help.

I made a board for my project.

I designed like that attach the image.

I connected Pin170(reset) and Pull up with the switch.

but voltage muresed always low signal(about 0.1V) at reset pin. so i think i can't debug using the JTAG.

can you plz check this port and my schematic.

- Jin

0 Kudos
Reply