How to ConfigurationPE micro JTAG?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to ConfigurationPE micro JTAG?

7,128件の閲覧回数
kbj8941
Contributor I

Hi Reader,

I have a S21K144EVB and a PE micro Multilink universal. 

I just want set up JTAG Debug without openSDA. 

I want to know configuration at S32 Design Studio for ARM Version 2018.R1.

I attach the setting image.  

タグ(4)
0 件の賞賛
返信
5 返答(返信)

6,997件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

it looks that you have swapped out JTAG cable. PIN #1 is on the Right side, not on the left as your image shows. 

Jiri 

0 件の賞賛
返信

6,998件の閲覧回数
kbj8941
Contributor I

Hi, Jiri

Thanks for reply.

I have some question,

 when don't it have openSDA schematic, how can i debbuger configuration using the multilink unviersal Fx with S32 studio?

0 件の賞賛
返信

6,998件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

Just choose Multilink FX probe in Debug configurations and connect JTAG cable. Make sure, that you have power for MCU (external 12V power supply or USB) - for USB J107 - shorted 2-3, for external power supply J107 - shorted 1-2 .

Jiri

0 件の賞賛
返信

6,998件の閲覧回数
kbj8941
Contributor I

i missed attach the image.

untitled.png

0 件の賞賛
返信

6,998件の閲覧回数
kbj8941
Contributor I

Hi,  Jiri

Thanks for reply.

i did it this problem!

but i have another prlblem. i need a your help.

I made a board for my project.

I designed like that attach the image.

I connected Pin170(reset) and Pull up with the switch.

but voltage muresed always low signal(about 0.1V) at reset pin. so i think i can't debug using the JTAG.

can you plz check this port and my schematic.

- Jin

0 件の賞賛
返信