How do I setup Toolchain for HSM core firmware development?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do I setup Toolchain for HSM core firmware development?

2,972件の閲覧回数
ktyong
Contributor I

When I select the MPC5748G processor in S32, there are only Z4 and Z2 cores in the Toolchain list.

HSM using Z0 core, how can I add Z0 core to Toolchain list?

タグ(4)
0 件の賞賛
返信
2 返答(返信)

2,382件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello,

Currently we do not support custom security code firmware development on the HSM therefore there is no support in S32DS New Project Wizard.

What we offer is SHE firmware security solution. This SHE firmware is pre-programmed on the HSM and the users can then use the HSM like a black box. You can then send commands from the host application to perform cryptographic functions.

Hope it helps.

Stan

0 件の賞賛
返信

2,382件の閲覧回数
bix010
Contributor III

Hi,

For a new MPC 5748G processor, do we need to enable the HSM by writing DCF records ourselves? Or does is the HSM already enabled by factory settings?

0 件の賞賛
返信