How do I setup Toolchain for HSM core firmware development?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I setup Toolchain for HSM core firmware development?

2,939 Views
ktyong
Contributor I

When I select the MPC5748G processor in S32, there are only Z4 and Z2 cores in the Toolchain list.

HSM using Z0 core, how can I add Z0 core to Toolchain list?

0 Kudos
Reply
2 Replies

2,349 Views
stanish
NXP Employee
NXP Employee

Hello,

Currently we do not support custom security code firmware development on the HSM therefore there is no support in S32DS New Project Wizard.

What we offer is SHE firmware security solution. This SHE firmware is pre-programmed on the HSM and the users can then use the HSM like a black box. You can then send commands from the host application to perform cryptographic functions.

Hope it helps.

Stan

0 Kudos
Reply

2,349 Views
bix010
Contributor III

Hi,

For a new MPC 5748G processor, do we need to enable the HSM by writing DCF records ourselves? Or does is the HSM already enabled by factory settings?

0 Kudos
Reply