How can i setup the S32K without SDK in S32DS?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can i setup the S32K without SDK in S32DS?

2,278件の閲覧回数
adrianwenger
Contributor III

I want to setup a project only with includedperipheral declarations from #S32K144.

How do i have to proceed?

タグ(2)
0 件の賞賛
返信
3 返答(返信)

2,067件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

I am not sure if I understand your question correct, but if you want to create project empty project for S32K144, click File->New->New S32DS project

pastedImage_1.png

Choose S32K144, insert project name and click next:

pastedImage_2.png

Do not change any settings on the following screen and click Finish

pastedImage_3.png

Regards,

Martin

0 件の賞賛
返信

2,067件の閲覧回数
adrianwenger
Contributor III

Hi Martin,

this Topic has already been resolved in the last week.

I don't know why it has apeared again as open...

Regards,

Adrian

0 件の賞賛
返信

2,067件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello Adrian,

I overlooked it. Maybe some database error. I am glad it was successfully resolved.

Regards,

Martin

0 件の賞賛
返信