How can i setup the S32K without SDK in S32DS?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How can i setup the S32K without SDK in S32DS?

2,280 次查看
adrianwenger
Contributor III

I want to setup a project only with includedperipheral declarations from #S32K144.

How do i have to proceed?

标记 (2)
0 项奖励
回复
3 回复数

2,069 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

I am not sure if I understand your question correct, but if you want to create project empty project for S32K144, click File->New->New S32DS project

pastedImage_1.png

Choose S32K144, insert project name and click next:

pastedImage_2.png

Do not change any settings on the following screen and click Finish

pastedImage_3.png

Regards,

Martin

0 项奖励
回复

2,069 次查看
adrianwenger
Contributor III

Hi Martin,

this Topic has already been resolved in the last week.

I don't know why it has apeared again as open...

Regards,

Adrian

0 项奖励
回复

2,069 次查看
martin_kovar
NXP Employee
NXP Employee

Hello Adrian,

I overlooked it. Maybe some database error. I am glad it was successfully resolved.

Regards,

Martin

0 项奖励
回复