How can I import [.dbc] files into an S32DS?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How can I import [.dbc] files into an S32DS?

2,483 次查看
alstlr926
Contributor III

Dear supporters

I control S32K144 using S32DS. I'm currently implementing a CAN communication system, and I have a question.
I have a [DBC] file, and I need to configure the source according to the message information in that [DBC] file. It doesn't matter if I only create a CAN system once, but if I do need to create multiple CAN systems, inputting the information from the [DBC] file is quite inefficient.
So I'm curious, is there any way you can call up [DBC] files from S32DS and extract the information inside them?
Ultimately, I want to create a function that allows me to set up buffers and store medium components on my own if I just import any [DBS] file.

Thank you.

Minsik.

0 项奖励
回复
1 回复

2,395 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

unfortunately I can't see such option in the Design Studio.

I saw, for example, that EB Tresos for Autosar/MCAL had such feature (licensed) but that's not the case of S32DS.

Regards,

Lukas

0 项奖励
回复