How To Solve The Build Errors about Create New Project from Example ‘RSDK_S32DS_template’

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How To Solve The Build Errors about Create New Project from Example ‘RSDK_S32DS_template’

4,141件の閲覧回数
jone_yang
Contributor II

HI,

   I follow the Step:"HOWTO: Create New Project from Example ‘RSDK_S32DS_template’" Create my Project successfully. Link: https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Create-New-Project-from-Example-...

 

but build all the project,Many errors occurred. How to solve it?

The RSDK version is 

 

yangliujie1_0-1661394695248.pngyangliujie1_0-1661394695248.png

 

yangliujie1_1-1661394749515.pngyangliujie1_1-1661394749515.png

 

 

ラベル(1)
タグ(1)
0 件の賞賛
返信
5 返答(返信)

4,105件の閲覧回数
jone_yang
Contributor II

i update the code for the projects by suggest,then build again.

the another errors occured! 

yangliujie1_0-1662363749684.pngyangliujie1_0-1662363749684.png

 

0 件の賞賛
返信

4,136件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

it looks like the files are not generated. You need to update the code for the projects:

lukaszadrapa_0-1661415910590.pnglukaszadrapa_0-1661415910590.pnglukaszadrapa_1-1661415931101.pnglukaszadrapa_1-1661415931101.png

Regards,

Lukas

0 件の賞賛
返信

4,103件の閲覧回数
jone_yang
Contributor II

 

add on the package :"BBE32 DSP Add-on package 1.2.0 for S32 Design Studio 3.4 Update 1",build again,then license error occured.

yangliujie1_0-1662364799304.pngyangliujie1_0-1662364799304.png

 

0 件の賞賛
返信

4,082件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

did you download and install LAX compiler? 

 

Jiri

タグ(1)
0 件の賞賛
返信

4,080件の閲覧回数
jone_yang
Contributor II

Hi, the LAX compiler installed

jone_yang_0-1662461326178.pngjone_yang_0-1662461326178.png

 

0 件の賞賛
返信