How I can use CMSIS in S32K Design Studio with S32K148(freeRTOS)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How I can use CMSIS in S32K Design Studio with S32K148(freeRTOS)

2,868 Views
Learner
Contributor III

Hi 
Is it possible to Integrate CMSIS with S32K Design Studio ?
If yes, Please share me the process to integrate CMSIS with S32K Design Studio.

Thanks 

0 Kudos
Reply
2 Replies

2,842 Views
Learner
Contributor III

Thanks @mikedoidge 
I will go through with the tutorial.

0 Kudos
Reply

2,853 Views
mikedoidge
NXP Employee
NXP Employee

Hello @Learner,

There is a great tutorial on using CMSIS here: https://mcuoneclipse.com/2013/02/14/tutorial-using-the-arm-cmsis-library/

It was written by our colleague @BlackNight. While the device is different and the tool (CodeWarrior) is different, the steps should be quite similar as the devices use ARM cores and the tools are built on Eclipse.

Best Regards,

Mike

0 Kudos
Reply