How I can connect Freemaster with Cyclone Fx?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How I can connect Freemaster with Cyclone Fx?

1,517 次查看
dk_mhlee
Contributor II

In Freemaster and Cyclone fx document, ODM is available.

I try to change configuration of Freemaster but it is not working

In the Freemaster, strange pop -up is comming on Option tap like below

pastedImage_1.png

But there are plugin object when I check the directory C:\Program Files (x86)\NXP\FreeMASTER 2.5\plugins\bdm

pastedImage_2.png

Please help me

2 回复数

1,437 次查看
dk_mhlee
Contributor II

Thanks~

When I update PEmicro & Cyclone drivers, the problem is solved

0 项奖励
回复

1,437 次查看
steven_mcgrath
Contributor II

Hello,

 

The DLL files that are in this location may be a little outdated. PEmicro will be able to provide you with the latest files that should get you up and running with the newest version of FreeMASTER. I would suggest visiting the homepage www.pemicro.com and going to the "Support" tab. Here you can setup a Support Request and a representative will be able to provide you with the necessary files once that is done.

 

Steve