HSM not working on S32-design studio

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HSM not working on S32-design studio

1,615 次查看
vladstoica
Contributor III

Hello,

 

I have a problem with the HSM module. In S32-design studio it cannot make two succesive encryptions or decryptions, only one of each. When I am making with the debugger, manually, it works fine, but in S32 the second encryption/deryption command doesn't work. What is the problem?

 

Vlad

标签 (1)
0 项奖励
回复
1 回复

1,405 次查看
coflynn
Contributor II

I'm just starting to experiment with this device for a design, and trying to even run code within the HSM. I see that you're (vladstoica‌) having similar issues to me w.r.t. getting the HSM up (no examples, can't compile stuff directly from HSM manual, etc). At this point I'm just trying to get code running on the Z0 core.

I have the security ref. manual but am trying to get a simple example running under S32 Design Studio... I was only sent the security ref without examples, so not sure if they even exist.

Did you have to manually get everything working within S32? Are you using OpenSDA (it doesn't even mention the z0 core), or just flash something into it and view the output?

0 项奖励
回复