FreeRTOS extension on S32 Design Studio 3.6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FreeRTOS extension on S32 Design Studio 3.6

1,319 次查看
Wolver
Contributor I

Hello everyone. I'm trying to use the latest FreeRTOS extension (SW32K3_FreeRTOS_11.1.0_5.0.0_CD1_D2409_DesignStudio_updatesite.zip) with S32 Design Studio 3.6, but every time that I add it to the source list nothing happens.

With S32 Design Studio I don't have this issue, I can easily import the .zip file and then immediately install the extension. I would use version 3.5 if I could, but for some reason I can only set it up on Windows, on Linux I can't get past the license check.

Given that I have to work on a Linux host and so S32 Design Studio 3.6 is my only available choice, how do I install the FreeRTOS extension?

Thanks in advance.

0 项奖励
回复
1 回复

1,279 次查看
RomanVR
NXP Employee
NXP Employee

Hi @Wolver.

Unfortunately, RTDs are not supported on a Linux host. The reason for this is that Linux is a case sensitive operative system which can cause conflicts within some filenames, although RTDs can be used, a proper functionality is not guaranteed.

This same topic is treated in the following post: "S32K3 SDK: Re-Attach RTD-SDK from command line", please let me know if the information is useful and we're sorry for the inconveniences.

- RomanVR.

Best Regards!
0 项奖励
回复