FreeRTOS extension on S32 Design Studio 3.6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FreeRTOS extension on S32 Design Studio 3.6

1,329件の閲覧回数
Wolver
Contributor I

Hello everyone. I'm trying to use the latest FreeRTOS extension (SW32K3_FreeRTOS_11.1.0_5.0.0_CD1_D2409_DesignStudio_updatesite.zip) with S32 Design Studio 3.6, but every time that I add it to the source list nothing happens.

With S32 Design Studio I don't have this issue, I can easily import the .zip file and then immediately install the extension. I would use version 3.5 if I could, but for some reason I can only set it up on Windows, on Linux I can't get past the license check.

Given that I have to work on a Linux host and so S32 Design Studio 3.6 is my only available choice, how do I install the FreeRTOS extension?

Thanks in advance.

0 件の賞賛
返信
1 返信

1,289件の閲覧回数
RomanVR
NXP Employee
NXP Employee

Hi @Wolver.

Unfortunately, RTDs are not supported on a Linux host. The reason for this is that Linux is a case sensitive operative system which can cause conflicts within some filenames, although RTDs can be used, a proper functionality is not guaranteed.

This same topic is treated in the following post: "S32K3 SDK: Re-Attach RTD-SDK from command line", please let me know if the information is useful and we're sorry for the inconveniences.

- RomanVR.

Best Regards!
0 件の賞賛
返信