Flashing multiply elf files with J-Link

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Flashing multiply elf files with J-Link

4,005 次查看
sebastian_wozni
Contributor III

Hello!

I want to flash multiply elf files in S32 Design Studio using SEGGER J-Link Ultra+ debugger and that is why I want to ask if there is possible to do that with this debugger. Previously I was using Multilink Universal FX from PE Micro and in configuration for this debugger there is possible to specify the number of additional object files I wish to program but in J-Link config there is no that kind of option. So my question is, is there any other option to use J-Link and flash 3 elf files in one session or is there any option to generate object file fields?

Thank you in advance!

Best regards,

Sebastian Wozniak

标记 (5)
0 项奖励
回复
2 回复数

3,486 次查看
njo
Contributor I

Hello,

Did you find a solution for this problem ?

Thank you in advance

 

Njo

0 项奖励
回复

3,832 次查看
jiri_kral
NXP Employee
NXP Employee

Hi Sebastian, 

I'm afraid that there is no such feature in Segger's eclipse (S32DS) plugin. May be you can find more info on Segger's forum:  J-Link/Flasher related - SEGGER - Forum  

Jiri 

0 项奖励
回复