Flashing multiply elf files with J-Link

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flashing multiply elf files with J-Link

3,961 Views
sebastian_wozni
Contributor III

Hello!

I want to flash multiply elf files in S32 Design Studio using SEGGER J-Link Ultra+ debugger and that is why I want to ask if there is possible to do that with this debugger. Previously I was using Multilink Universal FX from PE Micro and in configuration for this debugger there is possible to specify the number of additional object files I wish to program but in J-Link config there is no that kind of option. So my question is, is there any other option to use J-Link and flash 3 elf files in one session or is there any option to generate object file fields?

Thank you in advance!

Best regards,

Sebastian Wozniak

0 Kudos
Reply
2 Replies

3,442 Views
njo
Contributor I

Hello,

Did you find a solution for this problem ?

Thank you in advance

 

Njo

0 Kudos
Reply

3,788 Views
jiri_kral
NXP Employee
NXP Employee

Hi Sebastian, 

I'm afraid that there is no such feature in Segger's eclipse (S32DS) plugin. May be you can find more info on Segger's forum:  J-Link/Flasher related - SEGGER - Forum  

Jiri 

0 Kudos
Reply