Flashing multiply elf files with J-Link

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flashing multiply elf files with J-Link

3,988件の閲覧回数
sebastian_wozni
Contributor III

Hello!

I want to flash multiply elf files in S32 Design Studio using SEGGER J-Link Ultra+ debugger and that is why I want to ask if there is possible to do that with this debugger. Previously I was using Multilink Universal FX from PE Micro and in configuration for this debugger there is possible to specify the number of additional object files I wish to program but in J-Link config there is no that kind of option. So my question is, is there any other option to use J-Link and flash 3 elf files in one session or is there any option to generate object file fields?

Thank you in advance!

Best regards,

Sebastian Wozniak

0 件の賞賛
返信
2 返答(返信)

3,469件の閲覧回数
njo
Contributor I

Hello,

Did you find a solution for this problem ?

Thank you in advance

 

Njo

0 件の賞賛
返信

3,815件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi Sebastian, 

I'm afraid that there is no such feature in Segger's eclipse (S32DS) plugin. May be you can find more info on Segger's forum:  J-Link/Flasher related - SEGGER - Forum  

Jiri 

0 件の賞賛
返信