Facing issue in loading source files in S32DS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Facing issue in loading source files in S32DS

1,587 Views
Ankush_9881
Contributor II

Hello All,

   we are working on S32K146 on cmake based build system.we are able to compile the project successfully . Now we want to debug the .elf file on S32DS. We are able to to load the .elf in mcu at debug configuration but source file does not appear on the editor screen. It shows " no surce available for main()".

can anyone help me with this ?

Thanks

0 Kudos
Reply
1 Reply

1,566 Views
mikedoidge
NXP Employee
NXP Employee

Hello @Ankush_9881,

Could you please share a screen capture of the 'Debug Configurations' menu, 'Startup' tab for the configuration you used to program the ELF file?

What compiler did you use to build the ELF? Greenhills? GCC?

When you see this error, is there a button on the screen 'locate source code'?

Best Regards,

Mike

0 Kudos
Reply