FS32K148UJT0VLQT TCP/IP open source stack

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FS32K148UJT0VLQT TCP/IP open source stack

3,266件の閲覧回数
saad_saeed
Contributor III

Hello,

I am using FS32K148UJT0VLQT board with S32 design studio. Would you be kind enough to tell me, that whether, there is an open source TCP/IP stack available which can be ported on this board (I would prefer FNET). Your help will be appreciated.  

Regards,

Saad.

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,885件の閲覧回数
raresvasile
NXP Employee
NXP Employee

Hi,

LWIP TCP/IP stack is integrated in S32 SDK.

Best regards,

Rares

0 件の賞賛
返信

2,885件の閲覧回数
saad_saeed
Contributor III

Is there any way I can port FNET on this board?

0 件の賞賛
返信

2,885件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

you can try adapt fNET TCP/IP stack for kinetis MK64FN1M (it is similar to S32K148) - but have no idea how big effort it will be. 

2,885件の閲覧回数
saad_saeed
Contributor III

Yes, I agree. Both use ARM-CORTEX processor. 

If there is any information which can help me porting it, I Would be more than grateful.

0 件の賞賛
返信