Example projects for MPC5746B MCU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example projects for MPC5746B MCU

2,870 Views
jayasankar_band
Contributor I

Hi,

I cannot find example projects for MPC5746B MCU. I am using the latest S32DS V2.1 IDE.

Below are the list of example projects which I can see in S32DS.

pastedImage_1.png

Can you please help me to find the example projects for MPC5746B MCU ?

Or which one can I use in the existing list (mentioned in above screen shot) ?

Regards,

Jayasankar B

0 Kudos
Reply
4 Replies

2,794 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

there are examples only for main device from each family, not for all derivatives.

In case of MPC5746B, the 'parent' device is MPC5746C.

Regards,

Lukas

0 Kudos
Reply

2,794 Views
jayasankar_band
Contributor I

Hi Lukas,

Thanks for the reply.

As per my knowledge the 5746C is a dual core.

So, if I choose any of the projects related to 5746C, hope I don't need to change the anything related to the core configuration/startup code (Because the main core is same in 5746C and 5746B).

Can you please clarify this.

Regards,

Jayasankar. B

0 Kudos
Reply

2,794 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Jayasankar,

almost all examples are single-core only, so you can use them on MPC5746B. There are only some minor differences like number of CAN modules... So, you can use the examples for evaluation.

But when you are going to create your own application, I recommend to create new project using MPC5746B, of course.

Regards,

Lukas

0 Kudos
Reply

2,794 Views
jayasankar_band
Contributor I

Hi Lukas,

Sure. Thanks for the information.

Regards,

Jayasankar B

0 Kudos
Reply