Errors running builder 'CDT Builder' on project 'eepromflasher'. java.lang.NullPointerException

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Errors running builder 'CDT Builder' on project 'eepromflasher'. java.lang.NullPointerException

3,714 Views
alice_th
Contributor III

hello, 

when i use s32ds compile project, there some error below, could you help for this issue ? thanks

Errors occurred during the build.
Errors running builder 'CDT Builder' on project 'eepromflasher'.
java.lang.NullPointerException

 

15:46:43 **** Clean-only build of configuration STANDALONE for project eepromflasher ****
-j8 clean
Cannot run program "": Launching failed

Error: Program "" not found in PATH
PATH=[C:/NXP/S32DS_ARM_v2.2/eclipse/jre/bin/client;C:/NXP/S32DS_ARM_v2.2/eclipse/jre/bin;C:/NXP/S32DS_ARM_v2.2/eclipse/jre/lib/i386;C:\Windows\system32;C:\Windows;C:\Windows\system32\Wbem;C:\Windows\System32\WindowsPowerShell\v1.0\;C:\Windows\System32\OpenSSH;C:\Program Files\Common Files\Oracle\Java\javapath;C:\Program Files (x86)\VMware\VMware Player\bin\;C:\app\oracle\base\product\19.0.0\clienthome64_1\bin;C:\app\oracle\base\product\19.0.0\clienthome32_1\bin;C:\app\oracle\base\product\19.0.0\clienthome64_1;C:\app\oracle\base\product\19.0.0\clienthome32_1;C:\ProgramData\Oracle\Java\javapath;C:\Strawberry\c\bin;C:\Strawberry\perl\site\bin;C:\Strawberry\perl\bin;C:\platform-tools;C:\Python27;C:\Program Files\WindowsPowerShell\Scripts;C:\Program Files\MATLAB\R2021b\runtime\win64;C:\Program Files\MATLAB\R2021b\bin;C:\Program Files\MATLAB\MATLAB Runtime\v99\runtime\win64;C:\Program Files\MATLAB\R2020b\bin;%JAVA_HOME%\bin;C:\Program Files\dotnet\;C:\Program Files\Microsoft VS Code\bin;C:\Program Files (x86)\IVI Foundation\VISA\WinNT\Bin\;C:\Program Files\IVI Foundation\VISA\Win64\Bin\;C:\Program Files (x86)\National Instruments\Shared\LabVIEW CLI;C:\Program Files (x86)\IVI Foundation\VISA\WinNT\Bin;C:\Users\fshi\AppData\Local\Microsoft\WindowsApps;C:\Users\fshi\AppData\Local\Programs\Microsoft VS Code\bin;C:\Users\fshi\AppData\Local\Programs\Git\cmd;C:\Program Files\CMake\bin;C:\NXP\S32DS_ARM_v2.2\eclipse]

15:46:43 Build Finished (took 322ms)

alice_thanks_0-1704872874903.pngalice_thanks_0-1704872874903.png

alice_thanks_1-1704872921754.pngalice_thanks_1-1704872921754.pngalice_thanks_2-1704872946837.pngalice_thanks_2-1704872946837.png

 

 

0 Kudos
Reply
2 Replies

3,663 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

what S32DS version are you using? It looks that you are trying import project from S32DS for ARM v2.2 into S32DS v3.5. These versions aren't compatible. 

0 Kudos
Reply

3,708 Views
alice_th
Contributor III

can any nxp engineer help for this case, thanks a lot!

 

0 Kudos
Reply