Error when generating code for SCST Lib with S32K116, SDK 2.9.2 and IAR 8.22.2 c

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error when generating code for SCST Lib with S32K116, SDK 2.9.2 and IAR 8.22.2 c

1,979件の閲覧回数
tminh
Contributor I

Hello,

S32DS failed to generate SCST Library code with SDK S32K1xx_BETA_2.9.2 and IAR 8.22.2 compiler with below Error:

Description:   

Generator: FAILURE: at line 86: Unknown macro: "PE_G_XLKR_COMPILER" (file: Drivers\S32K\S32K144_SDK01\SCST.drv)

Location: scst2

Type: Processor Expert Problem

I could generate SCST successfully when not using IAR compiler.

Please help me to clarify this issue.

Thanks and Regards,

Minh

ラベル(3)
0 件の賞賛
返信
0 返答(返信)