Error sending an activation request to a remote activation server andprocessing .....

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error sending an activation request to a remote activation server andprocessing .....

726 次查看
david2023
Contributor I

Error sending an activation request to a remote activation server andprocessing the resulting response, A unigue license definition and a uniquelicense variation could not be determined for this product and entitlementline.

微信图片_20250401161144.png

0 项奖励
回复
2 回复数

678 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

there was issue on our license server which is already fixed. Please try to activate S32DS again. 

 

There is also new release of S32DS v3.6.1 with new features and without activation key.

0 项奖励
回复

711 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @david2023 

Other customers have experienced this type of error due to using the wrong activation code. Please verify that the activation code corresponds to the IDE version you are trying to install.

To find the correct activation code, follow these steps:

  1. Visit the S32 Design Studio 3.6.0 download page for Windows/Linux (S32 Design Studio 3.6 – Windows/Linux) → S32 Design Studio for S32 Platform v.3.6.
  2. Click on the "License Keys" tab to access your activation code. This will provide the activation key for the version you are installing.

To analyze other possible root causes, could you please share your log file? It can be found at C:\NXP\S32DS.3.6.0\_S32 Design Studio for S32 Platform 3.6.0_installation\Logs\S32_Design_Studio_for_S32_Platform_3.6.0_Install_MM_DD_YYYY (date)_HH_MM_SS(time).log

Note: These paths and steps may vary depending on the specific version of S32 Design Studio you are downloading. Also, to access the link I shared, you need to be logged into your account. Please make sure to log in before clicking the link.

 

BR, VaneB

0 项奖励
回复