Error loading .PCP file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error loading .PCP file

2,858件の閲覧回数
jjr_net
Contributor I

hello:

     I has a problem when I download program to S32R274 with flash Debug way. Err message below:

;begin_cs device=$00F98000, length=$001E8000, ram=$40000000
Loading programming algorithm ...
Error loading .PCP file : C:\NXP\S32DS_Power_v2017.R1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.8.3.201812312131\win32\gdi\P&E\nxp_s32r274_1x32x488k_cflash.pcp at address 40000060
Error loading programming algorithm - load aborted.
Error occured during Flash programming. 

 But download program with RAM Debug is OK.

 IDE is "S32 Design Studio for Power Architecture Version 2017.R1".

 

 Please help me, thank you!

タグ(3)
0 件の賞賛
返信
2 返答(返信)

2,682件の閲覧回数
steven_mcgrath
Contributor II

Hello,

The first thing I would try is to check to make sure that you have the most up to date plugin for S32 Design Studio, it seems yours may be a little older. To do so, navigate to the Help->Check for Updates and complete any necessary updates. Try restarting S32 Design Studio and perform the same test and see if you get the same result. I hope this helps!

Steve

0 件の賞賛
返信

2,682件の閲覧回数
jjr_net
Contributor I

hello, steve:

   According to you suggesetion,I updated S32, and the original problem has been solved.

thank you very much!

0 件の賞賛
返信