Error loading .PCP file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error loading .PCP file

2,831 Views
jjr_net
Contributor I

hello:

     I has a problem when I download program to S32R274 with flash Debug way. Err message below:

;begin_cs device=$00F98000, length=$001E8000, ram=$40000000
Loading programming algorithm ...
Error loading .PCP file : C:\NXP\S32DS_Power_v2017.R1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.8.3.201812312131\win32\gdi\P&E\nxp_s32r274_1x32x488k_cflash.pcp at address 40000060
Error loading programming algorithm - load aborted.
Error occured during Flash programming. 

 But download program with RAM Debug is OK.

 IDE is "S32 Design Studio for Power Architecture Version 2017.R1".

 

 Please help me, thank you!

0 Kudos
Reply
2 Replies

2,655 Views
steven_mcgrath
Contributor II

Hello,

The first thing I would try is to check to make sure that you have the most up to date plugin for S32 Design Studio, it seems yours may be a little older. To do so, navigate to the Help->Check for Updates and complete any necessary updates. Try restarting S32 Design Studio and perform the same test and see if you get the same result. I hope this helps!

Steve

0 Kudos
Reply

2,655 Views
jjr_net
Contributor I

hello, steve:

   According to you suggesetion,I updated S32, and the original problem has been solved.

thank you very much!

0 Kudos
Reply