Error installing S32_Design_Studio_for_S32_Platform_3.6.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Error installing S32_Design_Studio_for_S32_Platform_3.6.0

跳至解决方案
1,542 次查看
rick1964
Contributor II

I cant install S32 Design Studio for S32 Platform 3.6.0  on Windows 10 Pro.

There is a error entry in the installation log:

S32 Design Studio for S32 Platform 3.6.0(Install All Uninstaller Components)
Status: ERROR
Additional Notes: ERROR - Error writing LaunchAnywhere components (Access Denied)

There is some prolem with my activation code. 

It doesn't matter whether I use online or offline registration, the result is always the same: the installation process stops and ends when verifying the license.

 

Is there a solution for this?

Thanks,

Richard

0 项奖励
回复
1 解答
1,391 次查看
rick1964
Contributor II
 

In the end, it turned out that the problem was either with Windows or the installation software used, InstallAnywhere. My main disk C in Windows had only about 11GB of free space, so I planned to install the software on disk D, which had enough capacity. However, S32 Design Studio requires about 12.5GB of space for temporary files during installation. When I launched the installer S32DS_3.6.0_win32.x86_64.exe, an error message appeared (the screenshot in Czech is attached):

"There is not enough space for the complete installation. Please select a temporary folder to place the installer."

So, I selected a folder on disk D, but the installation always ended with the error described above. In the end, freeing up space on disk C helped – after I freed up a total of 13GB on disk C, the installation went as expected.

Problem solved.

Thanks,no space for complete installation.jpg

Richard

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,524 次查看
RomanVR
NXP Employee
NXP Employee

Hello @rick1964 

Please try running the S32DS installer with administrator rights and ensure that the activation code has no typos. This error is generally caused by user rights restrictions.

Please let me know if this is helpful.

- RomanVR.

Best Regards!
0 项奖励
回复
1,505 次查看
rick1964
Contributor II

Thanks, but

I've tried this several times. I delete the license using licfix, then run the installation and copy the activation code directly from the email to avoid any transcription errors. The result is always the same (see attachment). What's strange is that I successfully installed Studio on another older computer (running Windows 7) using the same code without any issues. On the computer where the installation fails, I already have S32 Design Studio for Arm installed, as well as other software (MUXpresso, FreeMaster)."

Best regards,

Richard

0 项奖励
回复
1,476 次查看
RomanVR
NXP Employee
NXP Employee

Hello @rick1964.

Similar situations have been discussed in the community before. Please take a look at the below community thread and let me know if the solution provided there was helpful to you.

Installation of S32DS V3.6 fails on Windows 11.

- RomanVR.

Best Regards!
0 项奖励
回复
1,392 次查看
rick1964
Contributor II
 

In the end, it turned out that the problem was either with Windows or the installation software used, InstallAnywhere. My main disk C in Windows had only about 11GB of free space, so I planned to install the software on disk D, which had enough capacity. However, S32 Design Studio requires about 12.5GB of space for temporary files during installation. When I launched the installer S32DS_3.6.0_win32.x86_64.exe, an error message appeared (the screenshot in Czech is attached):

"There is not enough space for the complete installation. Please select a temporary folder to place the installer."

So, I selected a folder on disk D, but the installation always ended with the error described above. In the end, freeing up space on disk C helped – after I freed up a total of 13GB on disk C, the installation went as expected.

Problem solved.

Thanks,no space for complete installation.jpg

Richard

0 项奖励
回复