Enable IAR plugin in already existing project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enable IAR plugin in already existing project

Jump to solution
2,494 Views
Catosh
Contributor IV

Hello, 

I would like to test my project using the IAR toolchain in S32DS but to me looks like only a brand new project can be configured to use IAR toolchain.

Do you have any hint on this point?

Thanks and best regards, 

L.

Tags (2)
0 Kudos
Reply
1 Solution
2,370 Views
mikedoidge
NXP Employee
NXP Employee

Hello Catosh‌,

Unfortunately, there isn't a fully automated method to do this. Probably your best option is going to be using the New Project Wizard to create a new project for IAR toolchain and then import your code.

Hope it helps,

Mike

View solution in original post

0 Kudos
Reply
2 Replies
2,371 Views
mikedoidge
NXP Employee
NXP Employee

Hello Catosh‌,

Unfortunately, there isn't a fully automated method to do this. Probably your best option is going to be using the New Project Wizard to create a new project for IAR toolchain and then import your code.

Hope it helps,

Mike

0 Kudos
Reply
2,370 Views
Catosh
Contributor IV

Hi Mike, 

ok, thanks for the support provided. 

0 Kudos
Reply