Enable IAR plugin in already existing project

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Enable IAR plugin in already existing project

跳至解决方案
2,516 次查看
Catosh
Contributor IV

Hello, 

I would like to test my project using the IAR toolchain in S32DS but to me looks like only a brand new project can be configured to use IAR toolchain.

Do you have any hint on this point?

Thanks and best regards, 

L.

标记 (2)
0 项奖励
回复
1 解答
2,392 次查看
mikedoidge
NXP Employee
NXP Employee

Hello Catosh‌,

Unfortunately, there isn't a fully automated method to do this. Probably your best option is going to be using the New Project Wizard to create a new project for IAR toolchain and then import your code.

Hope it helps,

Mike

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,393 次查看
mikedoidge
NXP Employee
NXP Employee

Hello Catosh‌,

Unfortunately, there isn't a fully automated method to do this. Probably your best option is going to be using the New Project Wizard to create a new project for IAR toolchain and then import your code.

Hope it helps,

Mike

0 项奖励
回复
2,392 次查看
Catosh
Contributor IV

Hi Mike, 

ok, thanks for the support provided. 

0 项奖励
回复