Development Project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Development Project

2,729件の閲覧回数
vicchang
Contributor I

S32ds can be like Visual Studio

access to ACF_DataDe TranslateVsdkUMatToAcfDataDesc ?螢幕快照 2018-01-10 下午12.30.21.png

Future development projects to Visual Studio or S32ds which one?

タグ(4)
0 件の賞賛
返信
3 返答(返信)

2,539件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

it looks like that you are using S32DS for Vision - but I don't understand your question. If you are developing software for S32V234 - the S32DS for vision is right choice for future project development. 

Jiri

0 件の賞賛
返信

2,539件の閲覧回数
vicchang
Contributor I

S32DS I want develop a custom kernel (slider window) scan image 

Use Apex HW accelerate  Just like Visual  Studio Project .

0 件の賞賛
返信

2,539件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi,

Yes, you can create and build your custom APEX kernel in S32 Design Studio for Vision.

I'd recommend you to start with a new APEX project using Graph tools.

Select File -> New -> Project:

pastedImage_1.png

pastedImage_3.png

Hope it helps.

Stan

0 件の賞賛
返信