Debug burning error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debug burning error

741件の閲覧回数
zenging
Contributor I

I use the S32K311 chip, and the burner uses the PE burner. But this error occurs when I select Debug after compiling the program.

6e7a10111aa39aed8484e6905850026.png6e7a10111aa39aed8484e6905850026.png
------------------------------
monitor setexceptioncatching 2033
monitor selectcore 0
"monitor" command not supported by this target.
continue
The program is not being run.
------------------------------

6e469c813fa342356c0c03cc842e24f.png6e469c813fa342356c0c03cc842e24f.pngfe0326fca54aa74d64177d4f86b45e9.pngfe0326fca54aa74d64177d4f86b45e9.png
This is how my burner is wired. I chose yes
TP3--Port-B-7
TP4--Port-B-9
TP5--Port-B-13
TP6--Port-B-5
TP7--Port-B-15
I also connected VCC and GND on both sides
I would like to ask how this kind of problem should be solved

0 件の賞賛
返信
0 返答(返信)