Debug A53 with Virtual memory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debug A53 with Virtual memory

2,058 Views
HSchill
Contributor I

I'm trying to debug a S32G274A Cortex-A53 core 0_0 with MMU turned on
Have anyone managed to read Virtual memory with the S32 Design studio and the S32 Debug probe?

The Memory Spaces view doesn't support 64 Bit virtual Addresses ... 
Can that be changed (in configuration) ?
As soon as more than 32-bits is entered in the dialog box the Select key get "grayed"
Screenshot_20220214_173328.pngScreenshot_20220214_173328.png

btw.
Peripheral - view works 
Disassembly - doesn't work when not having a flat map

Regards 
Hans

0 Kudos
Reply
2 Replies

2,023 Views
mikedoidge
NXP Employee
NXP Employee

Hello Hans,

We are investigating this issue. Could you please provide some sample application which has the MMU turned on so we could reproduce on our side and as well confirm possible solution would work for you?

Best Regards,

Mike

0 Kudos
Reply

1,993 Views
HSchill
Contributor I

Hi,
The easiest would probably to load any aarch64 linux-kernel
or a much smaller approach - little kernel 
it can be found at https://github.com/littlekernel/lk 

If you want I can send you a little kernel build for the S32G274A EVB 
that can be booted from u-boot or TF-A

Regards
Hans 

0 Kudos
Reply