DDR test validation don't work at S32 DS 3.6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR test validation don't work at S32 DS 3.6

4,057 Views
Tianxiang_Huang
NXP Employee
NXP Employee

Hi S32 DS team,

Using S32 Design Studio version 3.6.0, build ID 241128, on Windows 11. When running any (f.e. Firmware Init Test) for the DDR, get following error. Apparently S32G SDK scripts use python version 2, whereas the installation of S32 Design studio has python3(S32DS\build_tools\msys32\mingw64\bin) and python2(S32DS\build_tools\msys32\mingw32\bin).

Tianxiang_Huang_0-1737698680587.png

Seems the tool use python3 but the script is python2. 

How could you fix this bug, can S32DS DDR tool config which python version to use. Or update the DDR tool python script thanks!

BRs,

Tianxiang

Labels (1)
0 Kudos
Reply
9 Replies

3,409 Views
KMA
Contributor II

Hello S32DS team,

 

I am facing the same problem with S32DS 3.6.1, is there any solution to this issue? 

0 Kudos
Reply

3,402 Views
Tianxiang_Huang
NXP Employee
NXP Employee

Hi Mohamed, 

 

What RTD version is the customer using? Please check if the RTD version matches the S32DS.

Following is the analysis in the Jira ticket.

Tianxiang_Huang_1-1751592027760.png

 

BRs,

Tianxiang

0 Kudos
Reply

2,754 Views
arun_belamge
Contributor III

Hello.

I am facing the same issue.

Can you please point me to the exact Version of RTD as well as Design Studio?

My current DS3.5 is not able to install RTD Version 5 for some reason.

Thank you!

0 Kudos
Reply

3,967 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

please create JIRA ticket on our internal pages for this bug. It looks, that the python script is not properly ported from Python 2.7 to Python 3. 

0 Kudos
Reply

3,932 Views
Tianxiang_Huang
NXP Employee
NXP Employee

Got it, Thanks!

BRs,

Tianxiang

0 Kudos
Reply

2,691 Views
amerkle
Contributor II

@Tianxiang_Huang We are using the v3.6.2 of the S32 DS and the problem still exists. Would need a solution on v3.6.2 base. Is it solved at all?

0 Kudos
Reply

2,680 Views
arun_belamge
Contributor III
Hello.
For me the the following IDE and RTD worked:
Design Suite : S32DS v3.5.12 (Update 12)
RTD Version :
SW32_RTD_4.4_5.0.0_QLP04_D2511
SW32G_RTD_4.4_5.0.0_D2410.
Hope this helps.

BR
Arun
0 Kudos
Reply

2,641 Views
amerkle
Contributor II

Thanks Arun, I guess the v3.5.12 uses Python 2.7 and thats why it works. I don't know whether there is an impact by not using the v3.6.2 just for the validation of the DDR RAM configuration, that is configured in v3.6.2

0 Kudos
Reply

2,431 Views
Tianxiang_Huang
NXP Employee
NXP Employee

Hi Amerkle,

Are you target for the S32G DDR test?

So far, the recommended DS version for S32G RTD(including the DDR tool) is v3.5 update 13. 

Tianxiang_Huang_0-1764125471002.png

Please use the correct version. Thanks

 

BRs,

Tianxiang

0 Kudos
Reply