DDR test validation don't work at S32 DS 3.6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR test validation don't work at S32 DS 3.6

4,055件の閲覧回数
Tianxiang_Huang
NXP Employee
NXP Employee

Hi S32 DS team,

Using S32 Design Studio version 3.6.0, build ID 241128, on Windows 11. When running any (f.e. Firmware Init Test) for the DDR, get following error. Apparently S32G SDK scripts use python version 2, whereas the installation of S32 Design studio has python3(S32DS\build_tools\msys32\mingw64\bin) and python2(S32DS\build_tools\msys32\mingw32\bin).

Tianxiang_Huang_0-1737698680587.png

Seems the tool use python3 but the script is python2. 

How could you fix this bug, can S32DS DDR tool config which python version to use. Or update the DDR tool python script thanks!

BRs,

Tianxiang

ラベル(1)
0 件の賞賛
返信
9 返答(返信)

3,407件の閲覧回数
KMA
Contributor II

Hello S32DS team,

 

I am facing the same problem with S32DS 3.6.1, is there any solution to this issue? 

0 件の賞賛
返信

3,400件の閲覧回数
Tianxiang_Huang
NXP Employee
NXP Employee

Hi Mohamed, 

 

What RTD version is the customer using? Please check if the RTD version matches the S32DS.

Following is the analysis in the Jira ticket.

Tianxiang_Huang_1-1751592027760.png

 

BRs,

Tianxiang

0 件の賞賛
返信

2,752件の閲覧回数
arun_belamge
Contributor III

Hello.

I am facing the same issue.

Can you please point me to the exact Version of RTD as well as Design Studio?

My current DS3.5 is not able to install RTD Version 5 for some reason.

Thank you!

0 件の賞賛
返信

3,965件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

please create JIRA ticket on our internal pages for this bug. It looks, that the python script is not properly ported from Python 2.7 to Python 3. 

0 件の賞賛
返信

3,930件の閲覧回数
Tianxiang_Huang
NXP Employee
NXP Employee

Got it, Thanks!

BRs,

Tianxiang

0 件の賞賛
返信

2,689件の閲覧回数
amerkle
Contributor II

@Tianxiang_Huang We are using the v3.6.2 of the S32 DS and the problem still exists. Would need a solution on v3.6.2 base. Is it solved at all?

0 件の賞賛
返信

2,678件の閲覧回数
arun_belamge
Contributor III
Hello.
For me the the following IDE and RTD worked:
Design Suite : S32DS v3.5.12 (Update 12)
RTD Version :
SW32_RTD_4.4_5.0.0_QLP04_D2511
SW32G_RTD_4.4_5.0.0_D2410.
Hope this helps.

BR
Arun
0 件の賞賛
返信

2,639件の閲覧回数
amerkle
Contributor II

Thanks Arun, I guess the v3.5.12 uses Python 2.7 and thats why it works. I don't know whether there is an impact by not using the v3.6.2 just for the validation of the DDR RAM configuration, that is configured in v3.6.2

0 件の賞賛
返信

2,429件の閲覧回数
Tianxiang_Huang
NXP Employee
NXP Employee

Hi Amerkle,

Are you target for the S32G DDR test?

So far, the recommended DS version for S32G RTD(including the DDR tool) is v3.5 update 13. 

Tianxiang_Huang_0-1764125471002.png

Please use the correct version. Thanks

 

BRs,

Tianxiang

0 件の賞賛
返信