Create An ISP Project From Existing VSDK Graph in S32DS3.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Create An ISP Project From Existing VSDK Graph in S32DS3.1

1,469 次查看
751301185
Contributor II

Hi,

When I create an ISP Project From Existing VSDK Graph using S32DS3.1,code emit has been completed.

Expand the folders within Camera_test_Demo, A53_gen, src and inc, no the newly generated output files.

/home/lilei/NXP/S32DS.3.1/S32DS/tools/clt/isp/1.0.0/bin/runItByIDE.sh: 行 24: java: 未找到命令

Can anyone help me solve this problem? Thank you

pastedImage_1.pngpastedImage_2.png

/home/lilei/NXP/S32DS.3.1/S32DS/tools/clt/isp/1.0.0/bin/runItByIDE.sh   The contents of the script file are as follows:

pastedImage_3.png

pastedImage_4.png

标记 (3)
0 项奖励
回复
0 回复数