Conditional expression compiler bug?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Conditional expression compiler bug?

4,235 次查看
hrvojeerjavec
Contributor III

Hello,

I am using S32 design studio for power architecture with MPC5744P and I have been using the conditional statements.

The shortened code looks like this:

 

// variable declaration for the sake of type insight

float dutyCycle;

vuint16_t a, b, c;

uint16_t inv = FALSE;

//assign a value to variable a

a = (pSub->VAL1.R * dutyCycle);

//assign a value to variable b
b = (-((int16_t)(pSub->VAL1.R * dutyCycle)));

//assign a value to variable c using a and b -> correct value
c = (inv) ? a : b;

//assign a value to variable c using statements used for assigning a and b

//-> incorrectly returns 0
c = (inv) ? (pSub->VAL1.R * dutyCycle) : (-((int16_t)(pSub->VAL1.R * dutyCycle)));

 

The c variable will be assigned correctly when using a and b variables, but will be 0 if the values are entered directly in the conditional expression.

 

Do you know what this could be about?

标签 (1)
0 项奖励
回复
5 回复数

4,068 次查看
martin_kovar
NXP Employee
NXP Employee

Hi,

could you please create some simple working example, which demonstrates your issue and post it here? From the source code you shared, it is difficult to reproduce you issue, because I have to check assembly code in debugger.

Could you please also write me, which version of S32 Design Studio you use (1.0 or 1.1)?

Regards,

Martin

0 项奖励
回复

4,068 次查看
hrvojeerjavec
Contributor III

I have been using the S32 Design Studio 1.1. This is a working example that is showing the misbehavior:

typedef                   short   int16_t;
typedef          unsigned short  uint16_t;
typedef volatile unsigned short vuint16_t;
int main(void) {
    float dutyCycle = 0.2f;
    vuint16_t val1 = 8000;
    vuint16_t a, b, c;
    uint16_t inv = 0;
    for(;;) {
        //assign a value to variable a
        a = (val1 * dutyCycle);
        //assign a value to variable b
        b = (-((int16_t)(val1 * dutyCycle)));
        //assign a value to variable c using a and b -> correct value
        c = (inv) ? a : b;
        //assign a value to variable c using statements used for assigning a and b
        //-> incorrectly returns 0
        c = (inv) ? (val1 * dutyCycle) : (-((int16_t)(val1 * dutyCycle)));
        /* Loop forever */
    }
}‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

					
				
			
			
				
			
			
				
			
			
			
			
			
			
		
0 项奖励
回复

4,068 次查看
stanish
NXP Employee
NXP Employee

Hello,

I'd recommend not to rely on implicit integer conversion here.

Could you try to cast the operands explicitly:


(vuint16_t)(-((int16_t)(val1 * dutyCycle)));

I have seen different results on different compilers (GHS vs. IAR vs. GCC,...).

hope it helps 

Stan

4,068 次查看
hrvojeerjavec
Contributor III

Thank you, this does give the correct result, although I would like to be able to rely on implicit integer conversion.

Seems it wasn't a problem in all other cases.

0 项奖励
回复

4,068 次查看
martin_kovar
NXP Employee
NXP Employee

Hi,

I consulted your use case with my colleague, who is compiler expert and it seems it is really compiler bug. So I reported it and I hope it will be fixed soon.

Regards,

Martin