Compiling and Launching failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Compiling and Launching failed

ソリューションへジャンプ
13,808件の閲覧回数
at21
Contributor II

while compiling I am getting make not find in path.

but when I use CDT builder it works with some warning but not error.

 Same for FSL and GNU maker it is not compiling

 

 

for launching also it showing launching failed error

0 件の賞賛
返信
1 解決策
13,802件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

can you please share more details? What is your target MCU and S32DS Version? 

 

For correct build you need S32DS Application Project 

jiri_kral_0-1623244493842.pngjiri_kral_0-1623244493842.png

 

It is possible that you created C/C++ project. For debugging is best option Debug Configurations and choose your debugger and start debug session. 

 

Jiri

 

元の投稿で解決策を見る

8 返答(返信)
13,797件の閲覧回数
at21
Contributor II

Version: 2018.R1
Build id: 180326

0 件の賞賛
返信
13,791件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

It is possible share your project? What kind of project it is - did you created it from scratch or you are opening some older one? 

 

Jiri 

0 件の賞賛
返信
13,777件の閲覧回数
at21
Contributor II

I am importing the existing project.

 

 

Now.. I tried compiling. Using miscellaneous options in C/C++ build I am using  --save-temps option.. It compiled successfully. 

 

But processor expert code generator is not working to set pin configuration.

0 件の賞賛
返信
13,771件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

When you import the project - are there some warning messages - like Some version of SDK is not available? Such type of issues are mainly caused by importing project based on older SDK. 

 

Jiri 

13,754件の閲覧回数
at21
Contributor II

Now I am trying to update the software..

 

But it stucks at 80% for a long long time.

 

Please help @jiri_kral 

0 件の賞賛
返信
13,803件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

can you please share more details? What is your target MCU and S32DS Version? 

 

For correct build you need S32DS Application Project 

jiri_kral_0-1623244493842.pngjiri_kral_0-1623244493842.png

 

It is possible that you created C/C++ project. For debugging is best option Debug Configurations and choose your debugger and start debug session. 

 

Jiri

 

13,791件の閲覧回数
at21
Contributor II

always I am getting permission denied error.. I am loosing hope to solve this error .. Please help

0 件の賞賛
返信
13,793件の閲覧回数
at21
Contributor II

My target MCU is S32K144

 

Since I am importing already created project..

0 件の賞賛
返信