Code port to S32K controller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code port to S32K controller

2,649 Views
ambarishhundeka
Contributor III

Hi,

I need to port the code from Renesas to NXP (IAR compiler used for renesas development ).

the code has some compiler oriented directives , I am not getting how to change those directives to S32 design studio (gcc compiler)  support format.

Problem 1:

#pragma segment="bl_fsl_codearea_RAM"

#pragma segment="bl_blc_globaldata_RAM" __far

T_U32 __far *u32SegmentStartAddress;

T_U32 __far *u32SegmentEndAddress;

volatile T_BOOL boolInterruptFlagValue;

/* Clear BL_FSL_CODE_RAM */

u32SegmentStartAddress = __segment_begin("bl_fsl_codearea_RAM");

u32SegmentEndAddress = __segment_end("bl_fsl_codearea_RAM");

while (u32SegmentStartAddress < u32SegmentEndAddress)

{

*u32SegmentStartAddress = 0x00U;

u32SegmentStartAddress++;

}

Problem 2 :

#pragma dataseg="m_bl_std_faiRecdata_RAM"

__no_init StdFailurRecord_t gStdFailureRecord;

#pragma dataseg=default

the above code can be replace with  

__attribute__((section("m_bl_std_faiRecdata_RAM"))) StdFailurRecord_t gStdFailureRecord;

is this correct?

 

Problem 3:

#pragma constseg="m_blc_Configdata_start"      // IAR code

__root const ConfigData_t gConfigData =

const ConfigData_t gConfigData __attribute__((used)) =

{

   { 0xFFU,0xFFU,0xFFU,0xFFU,0xFFU,0xFFU,0xFFU,0xFFU}

};

#pragma dataseg=default;

 

I have replaced the code with

#pragma constseg="m_blc_Configdata_start"      // GCC code

const ConfigData_t gConfigData __attribute__((used)) =

{

   { 0xFFU,0xFFU,0xFFU,0xFFU,0xFFU,0xFFU,0xFFU,0xFFU}

};

#pragma dataseg=default;

is it correct?

Problem 4:

what can I replace far and near of  IAR in GCC compiler supportable format?

T_U32 __far *u32SegmentStartAddress; (IAR format).

I have gone through the gcc compiler reference manual and solved some of the compiler oriented directives errors,

the above directives are not getting how to solve.

kindly need your help in this.

Thanks in advance.

Regards,

Ambarish

Labels (1)
1 Reply

2,206 Views
stanish
NXP Employee
NXP Employee

Hi Ambarish,

GCC does not support #pragma for section placement.

For placing a code/data/const into a custom section GCC uses:

__attribute__ ((section(".MySection")))‍

The __attribute__((section())) statement has to be present by each object (variable, const, function) in contrast to #pragma

GCC also do not distinguish between code/data/const sections.

The linker script file shall define a custom section e.g.:

.MySection : 
{
   __MY_SECTION_START = .;     
   KEEP (*(.MySection))    /* KEEP: avoid dead stripping if an object is not referenced */ 
   __MY_SECTION_END = .;       
} > m_section‍‍‍‍‍‍‍‍‍‍‍‍

In your code you can use the linker script file symbols and use them to perform e.g. an initialization of the section:





__MY_SECTION_START);

* Regarding not initialized variable sections:

If you create a custom data section outside of ".data" section - the section is not initialized by the default startup routine. You should add the init sequence e.g. into init_data_bss() if you want to initialize your custom section.

* Regarding near/far keyword. AFAIK this is not supported by GCC. 

see e.g. the document below for more info:

HOWTO: Run a routine from RAM in S32 Design Studio  

hope it helps.

Stan

0 Kudos
Reply