Clock configuration : MCU is not supported

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Clock configuration : MCU is not supported

ソリューションへジャンプ
1,873件の閲覧回数
Changwoo82
Contributor II

Hello!

I'm using the S32K3X8 Evaluation board.

Though I'm trying to change the clock division, it is failed because of error "MCU is not supported".

How can I solve this problem? 

 

 

0 件の賞賛
返信
1 解決策
1,820件の閲覧回数
Changwoo82
Contributor II

It was caused by DRM in company.

it was resolved after decrypting the file 'S32V2xx.dsn.

 

Thank you.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,831件の閲覧回数
Changwoo82
Contributor II

Hello.

 

Thank you for answer. Unfortunately, I installed S32DS v3.5 and RTD for S32K358...

After posting this, I found the same issue with this. It was related with the DRM in laptop.

So, I need to check this point at first, then I'll get back.

0 件の賞賛
返信
1,855件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Which version of S32K3 RTD did you install for S32DS v3.5? Please install RTD that supports S32K358. What I installed is S32K3_M27X Real-Time Drivers Version 3.0.0 P07. I can change the clock division in the Clocks tool of S32CT.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
1,821件の閲覧回数
Changwoo82
Contributor II

It was caused by DRM in company.

it was resolved after decrypting the file 'S32V2xx.dsn.

 

Thank you.

0 件の賞賛
返信