Can't find a source file /fp-bit.c

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can't find a source file /fp-bit.c

2,830 次查看
fangzanbin
Contributor II

Can't find a source file at "/home/jbuilds/workspace/S32DS_ToolsGCC_E200/build_gnu/opt/freescale/ELvle/obj_gcc/powerpc-eabivle/fp/e200z4/libgcc/../../../../../src_gcc/libgcc/fp-bit.c"  Locate the file or edit the source lookup path to include its location 

 

 

hi,everyone  

  I create a new project about MPC5744P.this project I add 'math.h' file,but after run several times,project occurred a problem,I think the problem about I not correctly use S32DS .Problem like that:181863_181863.pngQQ图片20170418140510.png

 

Original Attachment has been moved to: MPC5744P-S32DS.rar

0 项奖励
回复
2 回复数

2,266 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

I searched S32 Design Studio installation folder and this file is not contained. This means we do not provide this source code.

Which line in which file causes this problem? When you load the project into the microcontroller, does this project work (with/without debugger)?

Could you please provide me more details?

Regards,

Martin

0 项奖励
回复

2,266 次查看
fangzanbin
Contributor II

Hi Martin,

Thanks for you reply,after run the program several times,finally I found the problem arised when run "while(x<=65535)"in the main function.But the problem seems to  have no effect on my project,and the project works  with debugger.

Regards,

Frank

0 项奖励
回复