Can someone give an example project on S32K148 EVB board?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can someone give an example project on S32K148 EVB board?

1,823件の閲覧回数
kongdetao
Contributor III

Can someone give an example project on S32K148 EVB board?

thanks!

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,687件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello kongdetao@saicmotor.com‌,

The latest update for S32DS for ARM Update 8 , contains BETA v2.9.2 of the S32K1xx SDK. Within this SDK are many example projects for the S32K148 which you can load into S32DS using the Create New Project from Example wizard.

pastedImage_5.png

Hope it helps,

Mike

0 件の賞賛
返信

1,687件の閲覧回数
kongdetao
Contributor III

Thanks, Mike!

        I have tested the example, it can't send can message on the S32K148 EVB Board, because the evb board has a transiver chip which wasn't configured correctly.

        So, whant I want is  an CANFD example on the S32K148 EVB :smileyhappy: 

0 件の賞賛
返信