Can not debug

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can not debug

633 Views
liyongfeng
Contributor III

Based on the log output, could you tell me how to resolve this issue?

0 Kudos
Reply
2 Replies

574 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hello @liyongfeng,

Failing to load .ARP file could mean various things. As a general check, can you confirm this board was able to be programmed before? And check if cable is connected properly.

Also check if the correct .ARP file is selected (if HSE is not installed in the device, select hse_disabled) in 'Debug Configuration' > 'Advanced Options'

Julin_AragnM_0-1787864422369.png

I suggest also trying to update PEmicro plugin through S32DS Extensions and Updates: 

Julin_AragnM_1-1787864479071.png

Are you using an external debugger, or is this through the OpenSDA interface? Try using an external debugger, either PEmicro, SEGGER, Lauterbach, etc.

Is this an NXP eval board, or is this your custom design? 

Best regards,
Julián

0 Kudos
Reply

582 Views
liyongfeng
Contributor III

没人能够答复吗?

0 Kudos
Reply