CCS to scan JTAG for S32R45

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CCS to scan JTAG for S32R45

2,815 次查看
PraveenKumar_K
Contributor II

Hi Team,

I am using S32 Debug probe with S32R EVK, I use the CCS.exe to check the S32 probe can connect to S32R CPU or not from CCS console window. 

below is the image, when I tried to check it.

CCS_server.PNG

  

 

"JTAG DAP ID is invalid". can anyone give me some suggestion on how to solve this S32 Debug Probe issue.

 

Thanks in advance..

 

标签 (2)
0 项奖励
回复
3 回复数

2,803 次查看
mikedoidge
NXP Employee
NXP Employee

Hello Praveen,

This script will be deprecated in future release. It has already been replaced by the 'Test Connection' buttion in the Debug Configurations menu. It was not maintained so it reports this invalid state. It is not a symptom of any other issue.

Best Regards,

Mike

2,793 次查看
PraveenKumar_K
Contributor II

Thanks for your reply. I used to check the 'Test Connection' button. It shows "The Board is Connected". But still I am not able to debug the with the probe, so I tried with that method to check the JTAG scanning.

 

Thanks.

0 项奖励
回复

2,725 次查看
mikedoidge
NXP Employee
NXP Employee

Hello,

Sorry for the long delay, is your EVB setup to boot from Linux BSP? If so, please change the setup so it does not boot Linux OS. If Linux BSP is running when S32 Debugger is trying to connect via JTAG, it could be interrupted. The S32 Debugger does not yet have Linux-aware debugging enabled.

Best Regards,

Mike

0 项奖励
回复