CAN handler development

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN handler development

ソリューションへジャンプ
5,628件の閲覧回数
shrutib
Contributor I

Dear Community,

I am using s32k144 EVB with s32 design studio version R1.2018. While calling CAN_init and CAN_deinit from ISR routine, the code got stuck into vPortEnterCritical(). Please find the attachment for more details. Looking forward to your reply.

 

タグ(4)
0 件の賞賛
返信
1 解決策
5,350件の閲覧回数
raresvasile
NXP Employee
NXP Employee

Hi Shruti,

CAN_Init and CAN_Deinit are using FreeRTOS API to create/destroy semaphores. This is the reason why the FreeRTOS flow will block into assert.

If CAN driver initialization and deinitialization are made outside of the ISR, then everything should work ok.

Best regards,

Rares

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
5,350件の閲覧回数
raresvasile
NXP Employee
NXP Employee

Hi,

Is your application using SDK? 

Thank you,

Rares

0 件の賞賛
返信
5,350件の閲覧回数
shrutib
Contributor I

Hi Rares,

Yes, RTM SDK v2.0.0, also using FreeRTOS v8.2.1 

Thanks,

Shruti.

0 件の賞賛
返信
5,351件の閲覧回数
raresvasile
NXP Employee
NXP Employee

Hi Shruti,

CAN_Init and CAN_Deinit are using FreeRTOS API to create/destroy semaphores. This is the reason why the FreeRTOS flow will block into assert.

If CAN driver initialization and deinitialization are made outside of the ISR, then everything should work ok.

Best regards,

Rares

0 件の賞賛
返信
5,350件の閲覧回数
shrutib
Contributor I

Hi Rares,

Currently we did the same as you told. It means there is no other way to call CAN_init and CAN_deinit through ISR. Thanks for your time.

Regards,

Shruti.

0 件の賞賛
返信