CAN_PAL_Example_S32K144

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN_PAL_Example_S32K144

Jump to solution
4,207 Views
Coding_Torque-SDRS
Contributor III

Hi Community Members!

                        I'm working on CAN PAL S32K144 example that you privided on the RTM - i came to know about that there is new board that you have provided in the documentation like - S32K144 MB. Could you guys please resolve this? I couldn't find out that exact board anywhere. And I've tried using 2 S32K144 EVB's one configured as Master and one as Slave, but couldn't able to communicate with each other.

 

The screenshot has been attached for your references from the Documentation.  

 

Thanks and Best Regards,

SDRS

Tags (3)
0 Kudos
Reply
1 Solution
4,162 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

S32K144 MB is motherboard from validation boards, you cannot purchase that, I think.

You should be able to run CAN_PAL_Example_S32K144 between 2 boards. Be sure you have followed example description. Boards have to be powered by external 12V and SBC must be in forced normal mode to have its CAN transceiver active (otherwise must be configured via SPI). 

BR, Petr

View solution in original post

2 Replies
4,163 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

S32K144 MB is motherboard from validation boards, you cannot purchase that, I think.

You should be able to run CAN_PAL_Example_S32K144 between 2 boards. Be sure you have followed example description. Boards have to be powered by external 12V and SBC must be in forced normal mode to have its CAN transceiver active (otherwise must be configured via SPI). 

BR, Petr

4,140 Views
Coding_Torque-SDRS
Contributor III

@PetrS Hi thanks for the support, Actually I figured out that I've not implemented the CAN termination resistors to make the CAN code work. Now its fine.

0 Kudos
Reply