Bootloader CAN

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Bootloader CAN

1,036 次查看
rehab_hassan
Contributor II

It flashed using CAN rbf " MPC5744P_S32DS_UART1_CAN0.rbf" when I changed the following 

flash_rchw : org = 0x00FA0000, len = 0x4
cpu0_reset_vec : org = 0x00FA0004, len = 0x4
delay_us : org = 0x00FA0008, len = 0x4
appkey_addr : org = 0x00FA000C, len = 0x4

But the applications doesn't work 

 

when I Flashed using serial UART 0 the previous version of the rbf "MPC574xP_S32DS_UART0_CAN0_OpenSDA_RevE.rbf"  

the application worked when I write as 

flash_rchw : org = 0x00FC0000, len = 0x4
cpu0_reset_vec : org = 0x00FC0004, len = 0x4
delay_us : org = 0x00FC0008, len = 0x4
appkey_addr : org = 0x00FC000C, len = 0x4

 

any help with that ?

Thank you

0 项奖励
回复
0 回复数