BCC_S32K144_Monitoring example, a red LED is displayed and an error occurs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BCC_S32K144_Monitoring example, a red LED is displayed and an error occurs

ソリューションへジャンプ
1,769件の閲覧回数
jj0371
Contributor I

Hi I am testing FRDM33772BSPIEVB and S32K144EVB-Q100. While checking the BCC_S32K144_Monitoring example, a red LED is displayed and an error occurs. The battery pack is not connected. Is there a way to check the code normally without the battery pack?

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 解決策
1,671件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jang,

The connection of a battery pack is not strictly required for getting the mentioned example working. However, the battery pack connector is used also for supplying the MC33772B device itself. Therefore, you should use at least pins X1-2 (POS_BATT) and X1-34 (NEG_BATT) of the battery pack connector to supply the device, e.g. by 12V.

Best regards,

Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,672件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jang,

The connection of a battery pack is not strictly required for getting the mentioned example working. However, the battery pack connector is used also for supplying the MC33772B device itself. Therefore, you should use at least pins X1-2 (POS_BATT) and X1-34 (NEG_BATT) of the battery pack connector to supply the device, e.g. by 12V.

Best regards,

Tomas

0 件の賞賛
返信