BCC_S32K144_Monitoring example, a red LED is displayed and an error occurs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BCC_S32K144_Monitoring example, a red LED is displayed and an error occurs

Jump to solution
1,698 Views
jj0371
Contributor I

Hi I am testing FRDM33772BSPIEVB and S32K144EVB-Q100. While checking the BCC_S32K144_Monitoring example, a red LED is displayed and an error occurs. The battery pack is not connected. Is there a way to check the code normally without the battery pack?

Labels (1)
0 Kudos
Reply
1 Solution
1,600 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jang,

The connection of a battery pack is not strictly required for getting the mentioned example working. However, the battery pack connector is used also for supplying the MC33772B device itself. Therefore, you should use at least pins X1-2 (POS_BATT) and X1-34 (NEG_BATT) of the battery pack connector to supply the device, e.g. by 12V.

Best regards,

Tomas

View solution in original post

0 Kudos
Reply
1 Reply
1,601 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jang,

The connection of a battery pack is not strictly required for getting the mentioned example working. However, the battery pack connector is used also for supplying the MC33772B device itself. Therefore, you should use at least pins X1-2 (POS_BATT) and X1-34 (NEG_BATT) of the battery pack connector to supply the device, e.g. by 12V.

Best regards,

Tomas

0 Kudos
Reply