Adding existing source file to a project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Adding existing source file to a project

Jump to solution
5,120 Views
danielkageff
Contributor I

i am using S32 Design Studio for ARM 2018.R1 and have created an application project.  I want to add some existing source files to the project but can't figure out how to do it.  How is it done?  Thanks

Tags (2)
0 Kudos
Reply
1 Solution
4,815 Views
danielkageff
Contributor I

I did that, but didn't see the file in Sources until I figured out that I had to right-click on the folder and selet 'Refresh'.  then it showed up and became part of the build.  thanks

View solution in original post

0 Kudos
Reply
2 Replies
4,815 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

you can for example drag and drop your source file or simply copy your sources into workspace/Project/sources and include folder. There is nothing special about it. 

pastedImage_1.png

Jiri

0 Kudos
Reply
4,816 Views
danielkageff
Contributor I

I did that, but didn't see the file in Sources until I figured out that I had to right-click on the folder and selet 'Refresh'.  then it showed up and became part of the build.  thanks

0 Kudos
Reply