Adding existing source file to a project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Adding existing source file to a project

ソリューションへジャンプ
5,062件の閲覧回数
danielkageff
Contributor I

i am using S32 Design Studio for ARM 2018.R1 and have created an application project.  I want to add some existing source files to the project but can't figure out how to do it.  How is it done?  Thanks

タグ(2)
0 件の賞賛
返信
1 解決策
4,757件の閲覧回数
danielkageff
Contributor I

I did that, but didn't see the file in Sources until I figured out that I had to right-click on the folder and selet 'Refresh'.  then it showed up and became part of the build.  thanks

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
4,757件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

you can for example drag and drop your source file or simply copy your sources into workspace/Project/sources and include folder. There is nothing special about it. 

pastedImage_1.png

Jiri

0 件の賞賛
返信
4,758件の閲覧回数
danielkageff
Contributor I

I did that, but didn't see the file in Sources until I figured out that I had to right-click on the folder and selet 'Refresh'.  then it showed up and became part of the build.  thanks

0 件の賞賛
返信