Adding existing source file to a project

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Adding existing source file to a project

跳至解决方案
3,903 次查看
danielkageff
Contributor I

i am using S32 Design Studio for ARM 2018.R1 and have created an application project.  I want to add some existing source files to the project but can't figure out how to do it.  How is it done?  Thanks

标记 (2)
0 项奖励
回复
1 解答
3,598 次查看
danielkageff
Contributor I

I did that, but didn't see the file in Sources until I figured out that I had to right-click on the folder and selet 'Refresh'.  then it showed up and became part of the build.  thanks

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,598 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

you can for example drag and drop your source file or simply copy your sources into workspace/Project/sources and include folder. There is nothing special about it. 

pastedImage_1.png

Jiri

0 项奖励
回复
3,599 次查看
danielkageff
Contributor I

I did that, but didn't see the file in Sources until I figured out that I had to right-click on the folder and selet 'Refresh'.  then it showed up and became part of the build.  thanks

0 项奖励
回复