ActivationID error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,298件の閲覧回数
fyw
Contributor IV

The S32DS version is V1.2, when i want to active it, it report an err as below. 

How can i solve this? Thank you very much!

pastedImage_1.png

タグ(3)
1 解決策
3,141件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi,

I've checked the license activation transactions and they all seems to be ok.

Have you installed S32DS on this particular machine?

It seems the machine is missing Trusted Repository service so the license activation layer cannot finish activation process.

I'd recommend you to install/re-install S32DS on this machine otherwise some License Activation services are missing.

If you get any errors during installation could you possibly post it here.

This will help us to find the root cause of this issue.

Thanks!

Stan

元の投稿で解決策を見る

2 返答(返信)
3,142件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi,

I've checked the license activation transactions and they all seems to be ok.

Have you installed S32DS on this particular machine?

It seems the machine is missing Trusted Repository service so the license activation layer cannot finish activation process.

I'd recommend you to install/re-install S32DS on this machine otherwise some License Activation services are missing.

If you get any errors during installation could you possibly post it here.

This will help us to find the root cause of this issue.

Thanks!

Stan

3,141件の閲覧回数
fyw
Contributor IV

yes   active with the administrator's authority will solve it 

0 件の賞賛
返信